Nexperia widens its offering of discrete components in miniature DFN packaging with side-wettable flanks

×

Nexperia widens its offering of discrete components in miniature DFN packaging with side-wettable flanks

April 27, 2022

Nijmegen -- Rugged and reliable devices are AEC-Q101 compliant and save board space

Nexperia, the expert in essential semiconductors, today announced its latest product additions to a growing range of discrete devices which it provides in leadless DFN packages with side-wettable flanks (SWF). These space-saving and rugged components help satisfy the needs of next generation applications in smart and electric vehicles. The AEC-Q101 range of devices available cuts across all Nexperia’s product groups and includes:

  • BC817QBH-Q and BC807QBH-Q series 45 V, 500 mA NPN/PNP general-purpose transistors in DFN1110D-3.
  • BAT32LS-Q and BAT42LS-Q general purpose Schottky diode in DFN1006BD-2
  • BAS21LS-Q high-speed switching diode in DFN1006BD-2 package.
  • PDTA143/114/124/144EQB-Q series 50 V 100 mA PNP Resistor-Equipped Transistor (RET) family in DFN1110D-3 package.
  • 2N7002KQB – 60 V N-channel Trench MOSFET and BSS84AKQB – 50 V, P-channel Trench MOSFET in DFN1110D-3 package.

Leadless DFN packages are up to 90% smaller than SOT23 packages and this helps to reduce the amount of board space required for the rapidly increasing number of electronic components being used in the latest vehicles. The side-wettable flank feature offers very reliable automated optical inspection (AOI) of solder joint quality. Nexperia’s DFN packages deliver excellent thermal performance with high Ptot and are also the most rugged in the industry passing extended lifetime and reliability tests.

"Nexperia pioneered side-wettable DFN and now offers the widest range of AEC-Q101 qualified discrete components in these miniature leadless packages”, states Mark Roeloffzen, Senior Vice President & General Manager of Nexperia’s Bipolar Discretes Business Group. “More than 460 different high-volume devices are available in the recently released DFN1412D-3, DFN1110D-3, and DFN1006BD-2 packages. By offering even more devices in these miniature packages, Nexperia provides design engineers with greater opportunities to make their designs future-proof, having an impact on the mobility of the future. The new technology has already seen success with design-in and commitment from major Tier 1 automotive suppliers”.

 

Samples and production quantities are available today. For more information, including product specs and datasheets, please visit www.nexperia.com/automotiveDFN

About Nexperia

Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. Headquartered in Nijmegen, the Netherlands, Nexperia annually ships more than 100 billion products, meeting the stringent standards set by the automotive industry. These products are recognized as benchmarks in efficiency – in process, size, power, and performance — with industry-leading small packages that save valuable energy and space.

With decades of experience in supplying to the world’s leading companies, Nexperia has over 12,000 employees across Asia, Europe, and the US. Nexperia, a subsidiary of Wingtech Technology Co., Ltd. (600745.SS), has an extensive IP portfolio and is certified to IATF 16949, ISO 9001, ISO 14001, and ISO 45001.

 

Nexperia: Efficiency wins.

For press information, please contact:

 

Nexperia

Petra Beekmans, Head of Communications & Branding

Phone: +31 6 137 111 41

Email: petra.beekmans@nexperia.com

 

Judith Schröter

Phone: +49 170 8586403

Email: judith.schroeter@nexperia.com

 

Publitek

Björn Oberhössel

Phone: +49 4181 968098-30

Email: bjoern.oberhoessel@publitek.com