Nexperia brings the benefits of clip-bonded FlatPower packaging to bipolar junction transistors

Nexperia brings the benefits of clip-bonded FlatPower packaging to bipolar junction transistors

July 16, 2025

Nijmegen -- CFP15B package offers a compact and cost-efficient alternative to MJD series in DPAK package

Nexperia today announced the expansion of its bipolar junction transistor (BJTs) portfolio by introducing 12 new MJD-style BJTs in clip-bonded FlatPower (CFP15B) packaging. This new offering released as MJPE-series addresses the ongoing industry demand for more power-efficient and cost-effective designs in both industrial and automotive applications. Compared to traditional DPAK-packaged MJD transistors, MJPE-parts in CFP15B deliver significant board space savings and cost advantages without compromising performance.

 

The new portfolio includes six automotive-qualified (e.g. MJPE31C-Q) and six industrial-grade types (e.g. MJPE44H11), with VCEO ratings of 50 V, 80 V, and 100 V, and collector currents (IC) of 2 A, 3 A, and 8 A. Both NPN and PNP variants are available. These BJTs complement Nexperia’s extensive CFP portfolio, which already includes a wide range of Schottky and recovery rectifier power diodes – another step toward standardizing footprints across multiple product categories streamlining PCB design and simplifying supply chains.

 

Used in diverse applications such as power supplies for battery management systems (BMS), on-board chargers in electric vehicles (EV), and back-lighting for video displays, the CFP15B-packaged BJTs maintain equivalent thermal performance (up to 175°C operation for automotive applications) while offering a 53% smaller soldering footprint. Furthermore, the clip technology of the CFP15B package supports exceptional mechanical robustness while also enhancing the electrical and thermal performance of these devices.

 

“As the industry transitions to multi-layer PCBs, a trend driven by the increasing popularity of high-performance microcontrollers, packaging has become a crucial part of the thermal system," according to Frank Matschullat, Product Group Manager Power Bipolar Discretes at Nexperia. “Modern CFP packaging technology, designed for multilayer PCBs, offers equal electrical performance in a considerably smaller footprint, helping to reduce part and overall system costs. Nexperia has substantially expanded its capacity to meet the increasing demand for CFP-packaged products that are essential for future-proofing automotive and industrial applications, including the MJPE series of BJTs.”

 

To learn more about Nexperia’s portfolio of bipolar junction transistors, visit: nexperia.com/MJPE

About Nexperia

Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 12,500 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.

 

For press information, please contact:

 

Nexperia

Anne Proch

Tel: +49 160 916 884 18

Email: anne.proch@nexperia.com

 

Publitek

Lucy Sorton

Tel: +44 07966 301949

E-mail: lucy.sorton@publitek.com