Keeping industry running

Companies and hardware engineers need to adapt and develop their designs, products and processes accordingly. Manufacturing automation requires machine-to-machine (M2M) communication, while human-machine-interfaces (HMIs) become portable. The result is power supplies and motor controls are required to become progressively smaller and more efficient.

At Nexperia we support all these trends. But it takes more to address the needs of Industrial and Power customers. It requires proven quality and stable high-volume supply alongside lifetime reliability and product longevity. By producing over 100 billion products annually across a broad portfolio of products and packages, Nexperia keeps the industry running.

Read more on our Blogs.

Our application handbooks

Logic Handbook

Logic Handbook

Product Features and Application insights (309 pages)
ESD Application Handbook

ESD Application Handbook

Protection concepts, testing and simulation (157 pages)
Factory automation

Factory automation

From manufacturing and process control to robotics, building management and medical systems – automation is today’s ‘key’ word. Because automation not only provides greater control, it makes the best use of available resources, 24/7. But that means efficient 12 V / 24 V / 48 V power supplies, soft-start and hot swappable devices, and extremely light but powerful motors. And with the rising number of sensors, actuators and electronic control circuits, it also means robust system protection and EMI filtering.

Advanced Support Tools

Experience how Nexperia is empowering innovation with our latest support tools.

Power & Energy

Growing pressure from society and increasing legislation for reduced CO2 emissions, is pushing industries from automotive to telecoms to invest in more efficient power conversion and increased electrification. Efficient power use is a key industrial challenge and a driver for innovation. In industrial infrastructure sectors operating high-load 24/7 systems, every bit of efficiency gain can have a significant impact on operating cost. It also means looking at and improving a whole range of power and energy applications from high-current Battery Management Systems right through to renewable power sources.

Electric Mobility

Electric Mobility

From forklift trucks and golf carts to ebikes, hoverboards and escooters – electric mobility is significantly changing the way we and goods move about. One thing all these mobility options have in common is their integrated electric motor and rechargeable battery cells, making them eco-friendly, zero-emission vehicles. Slim and space optimized designs with high power density are essential to support state-of-the-art concepts.

Power tools

From household appliances to power tools, powerful PWM driven brushless DC motors have become the norm. With such a diverse range, different applications require different optimizations. Often small battery driven applications need to be extremely efficient in terms of power, size and noise. Alternatively, balanced current-sharing can be key for large multi-cell mobility systems where multiple MOSFETs are used in parallel.

AI and datacenters

AI and datacenters

AI workloads are driving unprecedented growth in data center capacity, placing ever-greater demands on compute, storage, networking, and power infrastructure. As next-generation AI models become larger and more distributed, high-performance data centers will rely on ultra-fast data movement, low-latency interconnects, and highly efficient power delivery to maximize performance and scalability. Beyond raw processing capability, system-level efficiency is critical. Ensuring that GPUs, accelerators, memory and networking hardware can be deployed, upgraded and serviced with minimal disruption. Reliable, high-density infrastructure is fundamental to supporting the next wave of AI training, inference, edge intelligence, and real-time data-driven applications.

Using GaN FETs in 80 plus titanium power supply

Industrial power supply units come in different shapes and sizes, but one commonality is the need to be safe and efficient. To ensure…
Quick Learning

Using Power GaN FETs in AC-to-DC converters

Silicon AC/DC converters are widely used, but with the constant need to be smaller, cheaper and more power dense they can face significant issues, such as …
Quick Learning

The importance of SOA - Quick Learning

When a MOSFET is selected for a high-power designs, engineers often select a device based on its on-resistance. Lower on-resistance results in MOSFETs with …
Quick Learning

Understanding MOSFET datasheet parameters – Quick Learning

Selecting a MOSFET can typically require searching through large parametric tables within datasheets, and with the huge amount of power MOSFETs on offer…
Quick Learning

Quick Learning: Introducing Silicon Germanium (SiGe) rectifiers

Silicon Germanium (SiGe) rectifiers deliver cutting-edge high efficiency, thermal stability and…
Quick Learning

How can we inspire you?

Read our blogs on the latest industry developments

Related topics

Reliable high-volume supply chain management
Automation plays a role in virtually every system, which leads to a wide range of performance and specification requirements. With more than 10,000 product types and capacity for over 90 billion devices every year, Nexperia can match your long-term needs.

Long-term commitment
For some applications six months can feel like a lifetime but for others a decade can easily be the operational standard. Nexperia’s lifetime reliability and product longevity ensure that we are there to support you for the long-term.

Living with automation innovation
Understanding how to best innovate for industrial automation requires real insight into the business. As we design and build discrete semiconductor assembly equipment ourselves (ITEC) we definitely see the bigger picture.