Nexperia enhances Energy Harvesting portfolio with innovative PMIC reducing BOM cost

Nexperia enhances Energy Harvesting portfolio with innovative PMIC reducing BOM cost

January 07, 2025

Nijmegen -- Complete power management solution enables inductor-less designs

Nexperia is expanding its energy harvesting portfolio with the NEH71x0 power management IC (PMIC) family. This advanced PMIC line combines superior performance, cost-efficiency, and versatility, setting a new standard in sustainable design for low power applications. Unlike competing products, these devices eliminate the need for an external inductor, significantly reducing circuit board space and bill-of-materials (BOM) cost. It is available in a compact 4 mm x 4 mm QFN28 package. Applications include remote controls, key fobs, smart tags, asset trackers, occupancy sensors, environmental monitors, wearables, keyboards, tire pressure monitors, and any number of Internet of Things (IoT) applications.

These new PMICs represent a complete power management solution for energy harvesting: enabling engineers to extend battery life, recharge batteries or supercapacitors, and even eliminate batteries in certain designs, thanks to its cold start feature. With the NEH71x0 (NEH7100BU, NEH7110BU) PMICs, designers can choose from multiple ambient power sources such as light, kinetic/piezo or a temperature gradient. With an input power range from 15μW to 100mW, these high-performance energy harvesting ICs can convert energy with an efficiency of up to 95%. These devices include an on-chip maximum power point tracking (MPPT) adaptive algorithm to optimize the energy harvested, which adapts every 0.5 second, making the PMIC extremely responsive to changing environmental conditions.

The NEH71x0 family integrates a range of power management features to protect batteries and storage elements, including over-voltage protection, low-voltage detection, and over-current protection. The addition of a low dropout (LDO) regulator and USB charging further reduces the BOM cost and simplifies the design process. For greater functionality, the NEH7100BU variant includes I2C programmability and measurement readings, giving engineers additional flexibility and control in their designs.

“The NEH71x0 family addresses key challenges in energy harvesting by offering an inductor-less solution with integrated power management features,” said Simon van der Jagt, Energy Harvesting Product Group Leader at Nexperia. “This enables customers to lower costs while delivering an innovative solution for a wide range of applications. By optimizing battery life and reducing the need for costly, polluting battery replacements, the NEH71x0 contributes to a more sustainable future of electronics.”

NEH71x0 complements NEH2000, Nexperia’s first energy harvesting power management IC – a compact, low-BOM converter – by adding more advanced energy harvesting features and a new set of power management features, marking the next step in a growing roadmap of innovative inductor-less energy harvesting products.

To learn more about NEH71x0 PMIC family, follow the link to the Nexperia website: www.nexperia.com/energyharvesting

About Nexperia

Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 14,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications.


The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.

For press information, please contact:

Nexperia

Anne Proch

Tel: +49 160 916 884 18

Email: anne.proch@nexperia.com

 

Publitek

Lucy Sorton

Tel: +44 07966 301949

E-mail: lucy.sorton@publitek.com