AC/DC flyback controllers from Nexperia enable higher power density GaN-based flyback converters

AC/DC flyback controllers from Nexperia enable higher power density GaN-based flyback converters

October 17, 2024

Nijmegen -- Controllers improve power efficiency and also reduce standby power consumption

Nexperia today introduced a new series of AC/DC flyback controllers as the latest additions to its continuously expanding portfolio of power ICs. The NEX806/8xx and NEX8180x are designed for GaN-based flyback converters in devices such as power delivery (PD) chargers, adapters, wall sockets, strip sockets, industrial power and auxiliary power supplies, and other AC/DC conversion applications requiring high power density.

 The NEX806xx/NEX808xx are quasi-resonant/multi-mode flyback controllers which operate from a wide VCC range (10-83V), while the NEX81801/NEX81802 are adaptive synchronous rectifier controllers. These ICs can be used in combination with Nexperia’s NEX52xxx PD controllers and other discrete power device to deliver a turn-key flyback converter solution that optimizes the current sense voltage level and PFM mode, reduces standby power, and achieves high efficiency across the entire load range. The primary side controller can be used to drive a silicon MOSFET or GaN high electron mobility transistor (HEMT) directly, which helps to improve power density, while the synchronous rectification (SR) controller utilizes an innovative adaptive control method to eliminate the possibility of mis-conduction of switching device, thereby improving overall system reliability.

This family of flyback controller ICs employs the TSOT23-6 flip-chip package to deliver better thermal performance and which also helps to prevent accidental triggering of the over temperature protection (OTP) function. The control circuit also includes additional protection features, making it ideally suited for use in consumer and industrial flyback power supply designs.

To learn more about Nexperia’s flyback controllers, visit www.nexperia.com/ac_dc_controller

About Nexperia

Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 14,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every commercial electronic design in the world – from automotive and industrial to mobile and consumer applications. 
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
 

For press information, please contact:

Nexperia

Anne Proch

Tel: +49 160 916 884 18

Email: anne.proch@nexperia.com

 

Publitek

Megan King

Tel: +44 7855060775

E-mail: megan.king@publitek.com