Nexperia launches e-mode GAN FETs for low and high-voltage applications
May 10, 2023Nijmegen -- Industry’s only supplier to offer both cascode and e-mode GaN FETs
.jpg)
Nexperia, the expert in essential semiconductors, today released its first Power GaN FETs in e-mode (enhancement mode) configuration for low (100/150 V) and high (650 V) voltage applications. By augmenting its cascode offering with seven new e-mode devices, Nexperia now provides designers with the optimum choice of GaN FETs from a single supplier alongside its substantial portfolio of silicon-based power electronics components.
Nexperia’s new portfolio includes five 650 V rated e-mode GaN FETs (with RDS(on) values between 80 mΩ and 190 mΩ) in a choice of DFN 5x6 mm and DFN 8x8 mm packages. They improve power conversion efficiency in high-voltage, low-power (<650 V) datacom/telecom, consumer charging, solar and industrial applications. They can also be used to design brushless DC motors and micro server drives for precision with higher torque and more power.
Nexperia now also offers a 100 V (3.2 mΩ) GaN FET in a WLCSP8 package and a 150 V (7 mΩ) device in a FCLGA package. These devices are suitable for various low-voltage (<150 V), high-power applications to deliver, for example, more efficient DC-DC converters in data centers, faster charging (e-mobility and USB-C), smaller LiDAR transceivers, lower noise class D audio amplifiers and more power dense consumer devices like mobile phones, laptops, and games consoles.
GaN FETs offer the highest power efficiency with the most compact solution size in many power conversion applications, features which substantially reduce the bill of materials (BOM). As a result, GaN devices are increasingly entering mainstream power electronics markets, including server computing, industrial automation, consumer, and telecom infrastructure. GaN-based devices offer the fastest transition / switching capability (highest dv/dt and di/dt) and deliver superior efficiency in low- and high-power conversion applications. The outstanding switching performance of Nexperia’s e-mode GaN FETs is attributable to very low Qg and QOSS values, while their low RDS(on) enables more power-efficient designs.
With this release Nexperia now supply a broad offering of GaN FET products to suit the wide range of power applications best suited to the technology, including cascode devices for high-voltage, high-power applications, 650 V e-mode devices for high-voltage, low-power applications and 100/150 V e-mode devices for low-voltage, high-power applications. Furthermore, Nexperia e-mode GaN FETs are fabricated on an 8” wafer-line for increased capacity and qualified for industrial applications according to JEDEC standard. The expansion of its GaN device offering is a testament to Nexperia’s commitment to quality silicon and wide-bandgap technologies.
To learn more about Nexperia’s new 100 V, 150 V and 650 V e-mode GaN FETS, visit: nexperia.com/gan-fets
About Nexperia
Headquartered in the Netherlands, Nexperia is a global semiconductor company with a rich European history and over 15,000 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every electronic design in the world – from automotive and industrial to mobile and consumer applications.
The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, sustainability, and stringent industry requirements are evident in its extensive IP portfolio, its expanding product range and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.
For press information, please contact:
Nexperia
Petra Beekmans, Head of Communications & Branding
Phone: +31 6 137 111 41
Email: petra.beekmans@nexperia.com
Judith Schröter
Phone: +49 170 8586403
Email: judith.schroeter@nexperia.com
Publitek
Megan King
Tel: +44 7855060775
E-mail: megan.king@publitek.com