Nexperia MOSFETs deliver Best-In-Class Safe Operating Area and improved RDS(on) for Hot Swap designs

Nexperia MOSFETs deliver Best-In-Class Safe Operating Area and improved RDS(on) for Hot Swap designs

October 08, 2018

Nijmegen -- Ensures no compromise between protection and operating efficiency

Nexperia, the global leader in discretes, logic and MOSFET devices, today introduced the latest addition to its NextPower Live linear-mode MOSFET family, PSMN3R7-100BSE delivers a best-in-class combination of strong Safe Operating Area (SOA) and low RDS(on), and is ideally suited for hot swap, soft start and e-fuse applications. In order to manage the high in-rush current that can occur when swapping a server board or other pluggable system, or to ensure that a processor board is brought up smoothly, a MOSFET with high SOA is used in conjunction with a  hot swap controller. Previous generation parts have traded off SOA against RDS(on), whereas the new technology maximizes SOA without affecting RDS(on), thereby maintaining high operating efficiency levels.

Nexperia’s new PSMN3R7-100BSE MOSFETs improve SOA with a four-fold improvement in linear mode performance compared to standard technology, yet have a maximum RDS(on) of only 3.95 mΩ (3.36 mΩ typ.) – around 18% less than previous devices. These N-channel 100V devices are available in the D2PAK package, qualified to 175 OC. Devices are fully compatible with hot-swap controllers from all leading manufacturers

Comments Mike Becker, Nexperia’s product manager: “Server and communications infrastructure companies are packing more and more processing power onto their blades and rack-based systems, continually pushing up power requirements. Reliable hot-swap operation is essential to manage the in-rush currents experienced during start-up, but as power levels rise and efficiency requirements increase, then low RDS(on) is also becoming more important . NextPower Live MOSFETs from Nexperia, deliver benchmark combination of strong SOA and low RDS(on), allowing engineers to design ultra-rugged hot-swap solutions to manage the in-rush currents, whilst lower RDS(on) delivers the highest level of efficiency.”

More information on the new PSMN3R7-100BSE NextPower Live linear-mode MOSFET, including product specs and datasheet is available at https://www.nexperia.com/products/mosfets/power-mosfets/PSMN3R7-100BSE.html

About Nexperia

Nexperia, the former Standard Products division of NXP, is a dedicated global leader in Discretes, Logic and MOSFET devices. The company became independent at the beginning of 2017. Focused on efficiency, Nexperia produces consistently reliable semiconductor components at high volume: 90 billion annually. Our extensive portfolio meets the stringent standards set by the Automotive industry. Industry-leading, miniature packages, produced in our own manufacturing facilities, combine power and thermal efficiency with best-in-class quality levels.
With over 50 years history supplying to the world’s biggest companies, Nexperia has over 11,000 employees across Asia, Europe and the U.S., offering global support. The company has an extensive IP portfolio and is certified to ISO9001, ISO/TS16949, ISO14001 and OHSAS18001.

For press information, please contact:

Nexperia Agency: BWW Communications

Petra Beekmans, Head of Communications & Branding
Phone: +31 6 137 111 41
Email: petra.beekmans@nexperia.com

Nick Foot, director
+44-1491-636393
Nick.foot@bwwcomms.com